How thermostatic radiator valves increase boiler efficiency - VIDEO

Tuesday, July 19, 2022
EPBD Thumbnail
EPBD learning video

How thermostatic radiator valves can do wonders for condensing boiler efficiency

See how Danfoss Thermostatic Radiator Valves (TRVs) optimize the efficiency of condensing boilers in radiator heating systems. The efficiency is increased because TRV's lower the return temperature, supporting the condensing boiler to run in condensing mode most of the operation time. TRV's are the simplest and most effective solution for new EU regulations mentioned in the EPBD.