Our newest member of the smart home family just landed! Built on Zigbee technology, Danfoss Ally™ now speaks the same wireless language as tons of other smart home devices around the globe. Danfoss Ally™ also has an open API interface. The open API enables other energy players to get access to data and insights from the Danfoss expertise of heat regulation. This gives the end user the full smart home experience.
Electronic radiator thermostats are here to pave the way for future homes packed with energy intelligent technology. Besides from sporting a record-breaking 1 min reaction time on temperature changes, it can connect to home automation systems like Amazon Alexa and it comes with an App for remote control. You can also program schedules, so the heating adjusts automatically to the rhythm of the household, for example by lowering the temperature when you are at work or sleeping.
Optimizing the heat to follow the rhythm of the household provides the exciting opportunity for up to 30% energy savings. It’s an easy CO2-reduction potential just waiting to be tapped by homeowners all around the world. Furthermore, electronic radiator thermostats offer, programming, open-window detection and cool integration with homes that can save energy and increase comfort. Learn more about all the cool features.
Check out this short video below on some of the main benefits of the electronic radiator thermostats.
However, many heating professionals do not feel 100% comfortable selling this type of product yet, because of all the questions on use and technology homeowners may have. Don’t worry, we know you are not an IT specialist! We have tried to make it easier for you to recommend this product for households wanting to enter the 21st century and take full opportunity of the new digital options for smart heating.
Check out more about smart heating.
Electronic thermostats like the Danfoss Eco™, also comes with algorithms that adjusts for perfect hydronic balancing without you having to do a single pre-setting calculation or manual adjustment of the radiator valves. The balancing of water flow in the radiator system all happens automatically, as the Danfoss Eco™ both senses the temperature of the water in the pipes and the air temperature in the room. Knowing these two data points, it can adjust the flow of water of the valve very precisely according to the temperature setting.
The super-fast reaction time of 1 min. alerts the Danfoss Eco™ within 60 seconds on temperature changes, which allows it to quickly adjust for small imbalances before they become big noticeable temperature drops. This process also ensures out-standing comfort for homeowners, as the Danfoss Eco™ will feel and adjust for the smallest temperature fluctuations, often before the homeowner notices a difference in comfort. The result is homes in a constantly perfect temperature balance and reduced energy consumption.
The electronic thermostats run on batteries that will last for around 2 years under normal use conditions.
See more about how auto-balancing works with Danfoss Eco™ in the video below.