Green Renovations and Energy Efficiency

40% of the world's energy consumption is used in buildings. Almost half of all human energy consumption goes into our homes. We need to heat a lot smarter, and get more out of less to beat climate change. Here is a deeper insight into the solutions that can boost green renovation of buildings with energy efficiency optimizations across the full heating system - from the heat source to the radiators or floor heating in the individual rooms. 

Green Renovations and Energy Efficiency 7 Items